I.MX6UL DDR3 Script Aid

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I.MX6UL DDR3 Script Aid

I.MX6UL DDR3 Script Aid

Following docs(English or Chinese version) are also can be referred as a hand on guide.

Freescale i.MX6 DRAM Port Application Guide-DDR3

飞思卡尔i.MX6平台DRAM接口高阶应用指导-DDR3篇

Please find i.Mx6DQSDL LPDDR2 Script Aid through below link.

i.Mx6DQSDL LPDDR2 Script Aid

Please find i.Mx6DQSDL DDR3 Script Aid through below link.

i.Mx6DQSDL DDR3 Script Aid

Please find i.MX6SX DDR3 Script Aid through below link..

i.MX6SX DDR3 Script Aid

Any questions are welcome!

Change History:

0.02 - Add total 1Gbit density supporting.

标签 (1)
附件
评论
hkr

Is there a newer version of the file? I saw a presentation with 5 tabs and also ARM DS-5 support... (https://community.nxp.com/docs/DOC-331528 )

Thanks! hkr

Hello LinWang,

   Greetings of the day...

       We have a customized imx6ul board which is having the two RAM chips(MT41K512M8DA-107P) connected parallel and using one CS pin DRAM_CS0. is this script support to test the 1GB DDR stress and calibration? where can i find the 1GB density script.

Thanks & Regards

Ganesh.K

无评分
版本历史
最后更新:
‎02-24-2016 07:13 PM
更新人: