I.MX53 DDR3 Script Aid

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX53 DDR3 Script Aid

I.MX53 DDR3 Script Aid

This is a tool can generate a DDR3 script easily for i.MX53 and only need input several parameters based on using DDR datasheet and system architecture.

Please find i.Mx6DQSDL DDR3 Script Aid through below link.

i.Mx6DQSDL DDR3 Script Aid

Please find i.Mx6DQSDL LPDDR2 Script Aid through below link.

i.Mx6DQSDL LPDDR2 Script Aid

Please find i.Mx6SL LPDDR2 Script Aid through below link.

i.Mx6SL LPDDR2 Script Aid

Any questions are welcome!

添付
コメント

Hi  LinWang,

Could you update DDR stress test tool for i.MX53 same as i.MX6?

Best Regards,

Satoshi Shimoda

Sorry, I am not the owner.

As I know we don;t have such plan.

Hi LinWnag,

Thank you for creating the link.

It helps us.

Best Regards,

Satoshi Shimoda

As a convenience, I updated the document to add a tab for generating a script compatible with Lauterbach's TRACE32 software. As I don't seem to be able to attach it here, please feel free to contact me if you're interested.

The changes are actually fairly simple:

mem set 0x021b080c 32 0x00000000 # MPWLDECTRL0 PHY0

becomes:

Data.Set 0x021b080c %Long 0x00000000 ; MPWLDECTRL0 PHY0

Comments are ';', use "Data.Set" to write to memory, 32-bit values are preceeded by %Long, 16-bit by %Short.

(I also added comments to the MPWLDECTRLn registers in the script)

評価なし
バージョン履歴
最終更新日:
‎09-30-2014 01:09 AM
更新者: