Hello.
I am firmware developer.
I used a PN512 + NRF51822 u-com.
connected uart tx,rx.
I need to example source code about uart of pn512.
Thank you for reply.
However the library itself do not provide support for Serial(UART) bus connection for user space Linux driver.
tree NxpNfcRdLib/comps/phbalReg/src/
NxpNfcRdLib/comps/phbalReg/src/
├── KinetisI2C
│ ├── phbalReg_KinetisI2C.c
│ └── phbalReg_KinetisI2C.h
├── KinetisSPI
│ ├── phbalReg_KinetisSpi.c
│ └── phbalReg_KinetisSpi.h
├── LinuxKernelSpi
│ ├── phbalReg_LinuxKernelSpi.c
│ └── phbalReg_LinuxKernelSpi.h
├── LinuxUserI2C
│ ├── phbalReg_LinuxUserI2C.c
│ └── phbalReg_LinuxUserI2C.h
├── LinuxUserSpi
│ ├── phbalReg_LinuxUserSpi.c
│ └── phbalReg_LinuxUserSpi.h
├── LpcOpenI2C
│ ├── phbalReg_LpcOpenI2c.c
│ └── phbalReg_LpcOpenI2c.h
├── LpcOpenSPI
│ ├── phbalReg_LpcOpenSpi.c
│ └── phbalReg_LpcOpenSpi.h
└── phbalReg.c
7 directories, 15 files
Is the plan to support UART for NxpNfcRdLib?
For your information: PN512 reader board | NXP
There is software example:
NFC Reader Library v4.040.05.011646 R1 for PNEV512B including all software examples. (REV 3.9 )
https://www.nxp.com/downloads/en/software-support/SW2979.zip