Search the Community
Turn on suggestions
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
20,000 results
Sorted by:
06-28-2023
11:14 PM
Hello, This is the pic of pinmux.c file of enet_txrx_example of imx rt 1060. I want to ask how actually the values of pin configueration is decided. like 0xB0A9U I...
Labels
- Labels:
-
i.MXRT
03-01-2024
12:40 AM
Hello, I can't able to execute the below cmd. I have followed the procedures properly everything steps executed but facing issue in this step.(Followed this doc i.MX RT: Secure Boot Episode 1...
10-19-2022
12:33 AM
Hi everyone, Looking into the MX RT 1170 datasheet, it states clearly that the 1G port support RMII interface. However, it's not clear to me if the other ENET ports (10/100) support RMII as well....
10-22-2021
07:01 AM
Hi I am using an imx rt 1020 and try to send 9bit data over dma, but having trouble sending the 9th bit. status_t LPUART_SendEDMA(LPUART_Type *base, lpuart_edma_handle_t *handle, l...
Show results in replies (3)
-
...ommunity.nxp.com/t5/i-MX-RT-Crossover-MCUs/LPUART-hardware-bugs-framing-error-not-detected-and-blocks-i...
-
...ver uart with DMA // https://community.nxp.com/t5/i-MX-RT/mx-rt-1020-send-9bit-over-DMA/td-p...
-
Hello Hope you are well and I apologize for my delayed reply. Commonly the 9bit is used to s...
05-03-2023
01:20 PM
I am using pin GPIO_AD_11 as GPIO25 to connect to a pin of another chip. The pin on the other chip is required to be pulled up but according to the Hardware Development Guide, GPIO_AD_11 needs to b...
06-14-2021
06:43 AM
Hello everyone, I want to use the MX RT1170 evalboard as a rapid control prototyping system together with Matlab and Simulink and the model based design toolbox. My first step is to integrate an I...
07-22-2022
05:10 AM
Hello, I have tried to use the MX RT1050 - EVKB board to reconstruct the experiment presented in https://www.nxp.com/docs/en/application-note/AN12078.pdf (Measuring Interrupt Latency), b...
Show results in replies (4)
-
...PT2 - can you help me to identify a test point for a GPT2_COMPAREx on the MX RT1050 - EVKB board ? In m...
-
...n oscilloscope - I am unsure where (on the MX RT1050 - EVKB board) I can attach/connect the probe of m...
-
Hello, sending my project will not help to solve my problem - I need to know where can I attach m...
-
...ollows: In the MIMXRT1050-EVKB rev A1, the related point is: You can find, it is the JTAG/SWD r...
04-29-2022
12:06 AM
...bsp; P.S I am using i-mx RT1020-EVK and SDK version is 2.6.1
04-18-2023
09:53 PM
Dear All, We are using MX RT1024 with bare metal application for our prototype design. Now due to some requirement change we need to host a Linux or Android OS, preferably Linux. Does the p...
Labels
- Labels:
-
i.MXRT
08-23-2012
03:44 PM