コミュニティを検索
4 週間前
I have a project in S32 Design Studio 3.6.4 for S32 Platform with RTD and wan't to debug it with Freemaster 3.2. I use the S32K144EVB. Connection should be via LPUART 1 with PIN PTC6 and PTC7. I h...
11-03-2025
01:13 PM
Hi, I'm facing issues with CAN communication with the S32K144EVB which I hope some kind soul might be able to help me with. Setup as follows - S32K144EVB RevC - J107 set to 2-3 (e...
10-12-2023
03:36 AM
Dear nxp I have S32K144EVB as below. I connect J-link with S32K144EVB as below. and I have make `S32K144_Project_Hello.elf` so, I execute run but error d...
返信の結果を表示(4)
-
You need to power the S32K144EVB: J107 1-2 S32K144 powered by 12 V power s...
-
...tatus Indicator S32K144EVB D2 LED GREEN.png) If you don't Press and hold the Reset (SW5) when p...
-
...bsp;S32K144EVB. and Now only D2 led blink with green as below on attached IMG_0012.MOV &n...
-
Dear @Robin_Shen I have off-line meeting with @'James Lee' <james.lee@nxp.com&g...
03-21-2024
06:01 AM
Hello Community Members ! I'm presently working on CAN module in S32K144 EVB and looking for some support t...
ラベル
- ラベル:
-
General
10-12-2023
03:41 AM
Dear nxp I have a S32K144EVB I need to a schematic for this. thanks Bryan
07-19-2022
03:46 AM
Hello there, I am designing a project for EV Cluster. Where i am planning to send the data from #S32K144EVB# to #i.MXRT1170# to display it on my Display #RK055HDMIPI4MAO#. My plan is to use S32k144EVB...
2 週間前
Hello, I am working on LIN communication using S32K144EVB as the LIN Master, and I am testing with the NXP example: lin_master_baremetal_s32k144 Setup Master: S32K144EVB (LIN Master) S...
- タグ:
- S32K144LIN
返信の結果を表示(8)
-
...iscussion. I would like to share an update after further detailed debugging on the S32K144EVB LIN issue....
-
...ield from being transmitted? Please find the image I attached have signal coming from LIN from S32K144EVB...
-
Hello @danielmartynek Sir, Thank you for the detailed explanation regarding blocking and non-...
-
...JA1027 and the requirement to power the S32K144EVB from a 12 V supply through J16. I have now updated m...
-
...olCode=S32K144EVB-SCH-29248-C1 You don’t need any additional hardware modifications, just ensure t...
-
If you can confirm on the scope that the master sends a valid LIN header (break, sync, PID) at the ...
-
Hello @Prashanth1, You are currently using SDK drivers that are about seven years old. It’s...
-
Hello @Prashanth1, We no longer support the legacy SDK drivers. The only examples available...
12-06-2023
08:09 PM
Hello, I'm trying to design an extended board for the S32K144EVB. I don't know how to place the connectors to match up with the board. Are there Gerber files available?
11-17-2020
01:31 AM
Hi! I've a demo-board S32K144EVB-Q100 with Schematic Rev.C. I've downloaded the following archive "S32K144EVB-SCH-29248-RB1" and inside the Rev goes only to "B". Could you please send me the Rev.C...
返信の結果を表示(4)
-
Hi alisonluan, S32K144EVB schematic Rev.C has sent to you through support ticket. Best R...
-
Hi Robin_Shen, I have S32K144EVB-Q100 Rev.C too, Could you please send me the schematic Rev.C? T...
-
Hi , I have a demo board "S32K144EVB-Q100",too. Could you sent me the schematic Rev.C,please. T...
-
Hi Robin_Shen, I have a demo board “S32K144EVB-Q100 Rev.C”, too. Could you please send me the s...
08-08-2022
01:00 AM
recently, i'm trying to run the S32K144EVB. however,when i connect usb to this board with J104 2 3 closed, J107 2 3closed, I find ENABLE pin of u11 is 0. when i give it a 3.3V , 3 color led works, b...