wireless UART & ble

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

wireless UART & ble

582 次查看
Saoussen
Contributor I

Hi, I wanna asking if there is somebody can help me to write a program that can send accelerometer and gyroscopedata using uart and BLE with kw38 MCU Also this program will help the client to choose each type of data ( accelerometer/gyroscope) will be displayed in his device 

(Nanosense sensor) 

0 项奖励
1 回复

556 次查看
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

Could you please provide more details about your application's connections? Are the connections intended to be like one of the examples in the image below?

EduardoZamora_0-1657303328969.png

Please, take a look at Heart Rate Sensor (hrs) and Temperature Sensor (temp_sens) example projects inside the KW38 SDK (wireless_examples > bluetooth). These examples could be used as a base to develop your application, they are highly configurable, allowing the user to set some relevant parameters and change the information being transmitted.

Also, please consult KW38 Custom Profile, you can use this article as a reference for Custom Profile creation as it is needed for both the server and the client GATT services to match.

Regards,
Eduardo.

0 项奖励