what does "gHciCommandDisallowed_c" mean when use QTool to connect?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

what does "gHciCommandDisallowed_c" mean when use QTool to connect?

1,525 Views
shaw_gavin
Contributor II

Error Code: gHciCommandDisallowed_c  Source: gHciCommandStatus_c 

HCI opCode: 0x200d

Labels (1)
4 Replies

1,262 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello, 

Which device are you using ? And how are you getting the error code you are mentioning ? Could you please help me with more details ? 

Regards, 

Estephania 

0 Kudos
Reply

1,262 Views
shaw_gavin
Contributor II

Sorry, My English is poor.

My device is QN9080C which is running the demo(wireless_uart) ,and I want to connect with the QN9080A USB Dongle.

My Dongle work with the Connectivity QTool,it can scan the QN9080C successfully,and then,the error code occurred when I tried to let it connect with board.

Hope you can understand me~~

Thanks!

0 Kudos
Reply

1,262 Views
szlittle
Contributor II

Hi:

You need to stop scanning before connect. 

Li Yongyong

1,262 Views
shaw_gavin
Contributor II

Thanks,It's useful !

0 Kudos
Reply