w8997 FW CRC error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

w8997 FW CRC error

796 Views
chengeneg
Contributor II

When the W8997 driver module with kernel version 4.4.50 is installed on the arm platform, the driver cannot be loaded properly and a FW CRC error indicated by the helper is displayed. len = 0x0011, txlen = 17 Abnormal print, suspect whether the firmware is incorrect

, download the firmware for git clone https://github.com/NXP/imx-firmware.git command of NXP, NXP_FIRMWARE \ took imx - the firmware, NXP, FwImage_8997 directory firmware, don't know whether it is right, If no, provide the firmware download path

0 Kudos
Reply
5 Replies

791 Views
chengeneg
Contributor II

I do not know whether the driver of this version supports the PCIE W8997 NIC driver mwifiex-lf-6.1.36_2.1.0, or whether the W8997 NIC driver has other versions. If yes, please inform me where to download the driver

0 Kudos
Reply

780 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @chengeneg 

What is your meaning of NIC?

If you are using this driver: mwifiex-lf-6.1.36_2.1.0, it means you downloaded from our git hub:

https://github.com/nxp-imx/mwifiex/tree/lf-6.1.36_2.1.0

 

Am I right?

This driver version is supported on Linux kernel  4.4.50, and also support PCIE-UART interface for Wi-Fi and Bluetooth.

 

And about the FW, yes, you are right. You can download firmware from this git hub:

https://github.com/NXP/imx-firmware.git

 

We suggest you choose same version with driver.

 

Can you please let me know your host side platform? Are you using our I.MX series board?

 

Best regards,

Christine.

Tags (1)
0 Kudos
Reply

773 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @chengeneg 

Are you using arm 32 bit or arm 64 bit host plat form?

Did you put the firmware in /lib/firmware/nxp/ directory on your board?

And can you please provide me your loading Wi-Fi driver parameter and full dmesg logs for further checking?

 

Best regards,

Christine.

Tags (1)
0 Kudos
Reply

741 Views
chengeneg
Contributor II

 

1.平台使用高通平台的QSDK,32位的arm,内核版本为linux-4.4.50
2.驱动版本为网站下载的mwifiex-lf-6.1.36_2.1.0,固件也为该版本mwifiex-lf-6.1.36_2.1.0.firmware
3.驱动加载为insmod mlan.ko , insmod mlan.ko mod_para=nxp/wifi_mod_para.con drvdbg=0xa0037

需要知道根据日志显示是否为估计不匹配问题,如果为估计不匹配请提供固件下载路径,一下为日志消息


[ 5532.027649] wlan: Loading MWLAN driver
[ 5532.048153] wlan: Register to Bus Driver...
[ 5532.048395] vendor=0x1B4B device=0x2B42 rev=17
[ 5532.055880] Attach moal handle ops, card interface type: 0x204
[ 5532.064595] No module param cfg file specified
[ 5532.075201] rx_work=1 cpu_num=4
[ 5532.078523] Attach mlan adapter operations.card_type is 0x204.
[ 5532.116405] Request firmware: nxp/pcieuart8997_combo_v4.bin
[ 5532.119917] woal_init_fw_dpc 3913
[ 5532.125102] wlan_pcie_dnld_fw 4018
[ 5532.145663] FW CRC error indicated by the helper: len = 0x0011, txlen = 17
[ 5532.145859] FW CRC error indicated by the helper: len = 0x0011, txlen = 17
[ 5532.151592] FW download failure @ 0, over max retry count
[ 5534.155624] FW failed to be active in time!
[ 5534.155660] wlan_dnld_fw fail ret=0xffffffff
[ 5534.158624] WLAN: Fail download FW with nowwait: 0
[ 5534.163141] Config Space Registers:
[ 5534.167991] reg:0x00 value=0x2b421b4b
[ 5534.171134] reg:0x04 value=0x00100546
[ 5534.174949] reg:0x10 value=0x4800000c
[ 5534.178759] reg:0x18 value=0x4810000c
[ 5534.182242] reg:0x2c value=0x00000000
[ 5534.186016] reg:0x3c value=0x000001e8
[ 5534.189534] reg:0x44 value=0x00000008
[ 5534.193178] reg:0x80 value=0x10110000
[ 5534.196974] reg:0x98 value=0x00000000
[ 5534.200472] reg:0x170 value=0x0001001e
[ 5534.204106] FW Scrach Registers:
[ 5534.207898] reg:0xcf0 value=0xfedcba00
[ 5534.211142] reg:0xcf8 value=0x0
[ 5534.214698] reg:0xcfc value=0x0
[ 5534.317890] reg:0xcf8 value=0x0
[ 5534.317913] reg:0xcfc value=0x0
[ 5534.419852] Interface registers dump from offset 0xc00 to 0xcfc
[ 5534.419903] 00070621 00000000 c0000000 80000000 9c4730c0 00000000 00000000 00000000
[ 5534.424606] 00000000 00000000 ffffffff 00000000 00000000 00000000 00000000 00000000
[ 5534.432800] 00000011 00000000 00000472 000000e5 00000000 00000000 00001040 76543210
[ 5534.440359] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 5534.448063] a5a00420 040d1be0 01070f1a 5d7c0000 031f9121 00000000 000001e1 00000000
[ 5534.455784] 00078120 00058110 00000000 00000000 00000000 00000000 00000000 00000000
[ 5534.463496] 00010202 00000000 00000000 ffffffff 008003c3 c8701424 00000000 00000000
[ 5534.471234] 00000000 00000000 00000000 00000000 fedcba00 00000000 00000000 00000000
[ 5534.478975] woal_request_fw failed
[ 5534.486657] Firmware Init Failed
[ 5534.489852] woal_add_card 10848
[ 5534.496175] Free module params
[ 5534.496267] woal_pcie_probe: failed
[ 5534.499260] wlan_pcie: probe of 0000:01:00.0 failed with error -14
[ 5534.502747] wlan: Register to Bus Driver Done
[ 5534.508944] wlan: Driver loaded successfully

0 Kudos
Reply

730 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @chengeneg 

请用附件给出的firmware 文件,放在您板子的如下路径: /lib/firmware/nxp/

并同步检测一下 该路径下的wifi_mod_para.conf文件中,PCIE8997部分是否与如下内容一致?

PCIE8997 = {
cfg80211_wext=0xf
max_vir_bss=1
cal_data_cfg=none
ps_mode=1
auto_ds=1
host_mlme=1
fw_name=nxp/pcieuart8997_combo_v4.bin
}

加载Wi-Fi driver 参数:

insmod mlan.ko

insmod moal.ko mod_para=nxp/wifi_mod_para.con drvdbg=0xa0037

 

Best regards,

Christine.

Tags (1)
0 Kudos
Reply