qn9080sip use j-link

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

qn9080sip use j-link

2,187件の閲覧回数
1758793535
Contributor I

 when I try to use " program lpc-link2 with segger j-link " to update the firmware, it will quit directly,so what should i do to make it show  fig3   BKAH(I[]AP}AE5BWVDD8WUM.pngjlink.pngCX8JZTZ0RFCUQNQ)5CMNOKD.png

0 件の賞賛
返信
15 返答(返信)

2,183件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

Before you update the firmware, you should use jumper to connect jp5. When update successfully, remove it.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

2,179件の閲覧回数
1758793535
Contributor I

hi

I did it, but it still doesn`t work. window of  "Program LPC-Link2 with Segger J-Link" quit directly .Is it connected like thislianjietu.jpg

0 件の賞賛
返信

2,171件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

Do you connect the jumper without power? 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

2,168件の閲覧回数
1758793535
Contributor I

Yes, i connected jumper without power. Do I need an emulator?

0 件の賞賛
返信

2,161件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

Update your lpcscrypt. lpc 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

2,156件の閲覧回数
1758793535
Contributor I

11.pngthankyou a lot  ,  i tried it again, but it showed me another problem. sorry ,could you tell me how to deal with it?

 

22.png

 

0 件の賞賛
返信

2,150件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

This is the problem of the PATH environment variable. Adding the directory of the windows command to the PATH will overwrite. That is: append to the path: %SystemRoot%\system32;%SystemRoot%;

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

2,145件の閲覧回数
1758793535
Contributor I

I have tried my best to do ,but it still someting wrongBL5%A(8Q$39RL$6{C3)YN83.png

0 件の賞賛
返信

2,135件の閲覧回数
nxf56274
NXP Employee
NXP Employee

3.PNG

0 件の賞賛
返信

2,128件の閲覧回数
1758793535
Contributor I

{A4ZQP]T)S5Q}%OFZ3P}6R6.pnghi ,it stope in here, and nothing happen.

0 件の賞賛
返信

2,102件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

Do you press  'space' to start update?

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

2,098件の閲覧回数
1758793535
Contributor I

Hi,

Yes,  i  pressed the "space", it just moved to the next line.

Have a great day,

0 件の賞賛
返信

2,093件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

Does your board work well? Can you download the program? If you do not connect the board, then press 'space', does it show something?

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

2,089件の閲覧回数
1758793535
Contributor I

hi

yes,i can download program from IAR by CMSIS-DAP  but cann`t use JLINK.

0 件の賞賛
返信

2,078件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

Please go to '

Control Panel\Hardware and Sound\Devices and Printers'. Do you see something like this? 

2.PNG

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信