qn9080sip Bluetooth connect problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

qn9080sip Bluetooth connect problem

484件の閲覧回数
boboyxu
Contributor I

Hi,

     I bought the qn9080sip development Kit,and when I use the qn9080sip to connect to my Android phone,I can monitoring  the connection status through the USB interface on the development board, the connection status is shown like this:000.png 

The qn9080sip can find my Android phone , BUT it will  disconnect very soon.

Could you tell me what is the problem? thank you very much!

0 件の賞賛
1 返信

464件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

Please refer this link QN9080SIP .

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛