The maximum number of child nodes of the coordinator (router) to set?
Hello,
The modification should not be done in the .h file, it is needed for you to modify it in the following way.
Regards,
Estephania
JN5189 zigbee3.0 stack
SDK_2.6.1_JN5189 middleware wireless zigbee
I found that the ZPS_CHILD_TABLE_SIZE parameter in the zps_gen.h file should set the number of child nodes,But the zps_gen.h and zps_gen.c file is a read-only file ,I want to know how to modify the parameters in the file.
For example,Modify the ZPS CHILD TABLE SIZE parameter to the maximum value.
Hello,
Which device are you using ? Also could you please share with me the protocol to be used?
Regards,
Estephania
JN5189 zigbee3.0 stack SDK_2.6.1_JN5189 middleware wireless zigbee I found that the ZPS_CHILD_TABLE_SIZE parameter in the zps_gen.h file should set the number of child nodes,But the zps_gen.h and zps_gen.c file is a read-only file ,I want to know how to modify the parameters in the file. For example,Modify the ZPS CHILD TABLE SIZE parameter to the maximum value