what's the flash/ram usage, about lib_ble_5-0_host_cm0p_gcc.a and lib_ble_kw36z_controller_gcc.a
I need do a evaluation for the chip
is there some doc for reference, about the usage?
Hi @frank-li2021,
I hope you are doing great.
Please look at the release notes that we provide on the SDK.
"\SDK_2_2_9_FRDM-KW36\docs\MCUXpresso SDK Release Notes_MKW36Z4.pdf" for example.
It also will depend on the example that you are working on, and the role that you want.
Regards,
Mario
thant you for your reply
but I don't find the docs, while I'm creating the project with mcuXpresso IDE
there're only some docs about freertos under the doc folder
please attach the link of releaes note, I'll check the flash/ram usage in it
Hi @frank-li2021,
Please look at the next image, the doc folder is could be download it.
Regards,
Mario
thank you so much
Hi Da Li
目前有资料说明 BLE lib 和 controller LIB 占多少 flash 和 ram 空间吗
我编译了一个 shell 的 demo ,从 map 文件分析,这两个库占了160+ 的 flash,这个数据对吗
或者有其他 资料可以参考,请帮忙 share 下 多谢