Hi, i use the pin DO0 to generate PWM,my code is below,but it does not work.
--project: JN-AN_1217-Zigbee-3-0-Base-Device
--ROUTER
PUBLIC void tim2_PWMInit(void)
{
vAHI_TimerSetLocation(E_AHI_TIMER_2,FALSE,TRUE); // PWM2
vAHI_TimerFineGrainDIOControl(1<<4);
vAHI_TimerEnable(E_AHI_TIMER_2,10,FALSE,FALSE,TRUE);
vAHI_TimerConfigureOutputs(E_AHI_TIMER_2,TRUE,TRUE);
vAHI_TimerClockSelect(E_AHI_TIMER_2, FALSE, TRUE);
vAHI_TimerStartRepeat(E_AHI_TIMER_2,1000,1000);
}
Hi Dylan,
Please see the code below, I already tested I am using the DIO8, Did you set the direction of the DO0 pin?.
vAHI_DioSetDirection(0, (1<<8));
vAHI_DioSetOutput(0,(1<< 8));
vAHI_TimerFineGrainDIOControl(0x9F);//Timer 3 and 4 enable
vAHI_TimerSetLocation(E_AHI_TIMER_4,TRUE,FALSE);
vAHI_TimerEnable(E_AHI_TIMER_4, 4,FALSE, FALSE, TRUE);
vAHI_TimerClockSelect(E_AHI_TIMER_4,FALSE, TRUE);
vAHI_TimerConfigureOutputs(E_AHI_TIMER_4,FALSE ,TRUE);
vAHI_TimerStartRepeat(E_AHI_TIMER_4,125 ,255);
// PWM_PERIOD = (1000000/1000)
Regards,
Mario
Hi Mario, i have anther problem,
--project: JN-AN_1217-Zigbee-3-0-Base-Device
--ROUTER
1.If DO2 connect to GND, the system fails to start;
2. If i take out the "R1",the system will start normal;
Hi Dylan,
The DO0 pin is only output purpose. I am not sure if you are programming but it should be floating.
Regards,
Mario
Hi mario, the application schematic diagram below, the mark "ZB_IRTX"connect to the DO0;
SO the DO0 generate PWM to drive the LED;
problem:the system can't start. But if take out the "R20",the system can start normal;
By the way, i make a test, if i connect the DO0 to the GND,the system also can't start;
Hi Dylan,
Please re-recalculate the resistance value that is connected to the DO0.
I suggest less value.
Regards,
Mario