Hello,
I want to use the OpenThread stack on the FRDM-KW41Z, I started by building and generating the binary files, thereafter I flashed the binary file on FRDM-KW41z through (PE micro) Test Tool (nxp), when I want to connect to the bus uart (ttyACM0) to control the communication of Thread nothing happens as expected, openthread/examples/platforms/kw41z at master · openthread/openthread · GitHub binary file as attachment, Best regards, Aymane
Hello,
Yes, I'm sure it's him is the good port used, indeed I have this port that is added after the
flash in /dev/tty*,
Regards,
Aymane
Hello,
thank you for your feedback,
I find the well UART port (/dev/ttyACM0) after the flash of the binary file,eventually I connect to this port, but I don't see anything and I can't write anything in the terminal,
Regards,
Aymane
Hello,
But are you sure that it's the one of the board you are using? Sometimes it gets enumerated in a different way.
Regards,
Estephania
Hello,
no, the binary file (.bin) is correctly flashed with 'Firmware Loader', and it demand me to unplug and plug the board, I tested to flash other binary file for other appli for example 'examples_bluetooth_wireless_uart' and it well worked.
Regards,
Aymane
Hello,
So, when you mention that nothing happens as expected, do you mean that you can't connect to the UART terminal? Or that you do not see anything or can't write something in the terminal? Are you sure you are opening the correct COM port?
It is most likely that you can find the solution to your questions by asking directly to the developers of the open thread stack as mentioned here
Regards,
Estephania
Hello,
Do you have an error in the Test Tool when flashing the files ?
Regards,
Estephania