Hi nxp:
The path is:
C: \ NXP \ bstudio_nxp \ SDK \ \ Jacqueline Nottingham - SW - 4170 Components \ ZCIF \ Source
and the file is:
zcl_reportManager.c
there is a function called:
eZCLCheckReportingConfigurationRecord
as below
This position is doing parameter check, when checking the maximum time interval, why is it illegal when it is less than but not greater than?
Hi Zhang,
Please look at the https://www.nxp.com/docs/en/user-guide/JN-UG-3077.pdf
B.7 Profile Initialisation of Attribute Reporting
Regards,
Mario
Hi Mario,
I looked at the document you said, but I didn't get the answer.
My question is that shouldn't we use the ">" here, rather than "<"
Because this location is compared to ZCL_Cmmon MAX interval,only if we pass in parameters beyond the ZCL_Cmmon MAX interval, it is E_ZCL_ERR_INVALID_VALLUE
Hi Zhang,
Thank you for your feedback, it should be like you suggest.
I am already reported.
Regards,
Mario
I looked at the document you said, but I didn't get the answer.
My question is that shouldn't we use the ">" here, rather than "<"
Because this location is compared to ZCL_Cmmon MAX interval,only if we pass in parameters beyond the ZCL_Cmmon MAX interval, it is E_ZCL_ERR_INVALID_VALLUE