Where can i download Freescale_802.15.4_MAC_PHY_V50.mcp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can i download Freescale_802.15.4_MAC_PHY_V50.mcp

256 Views
YJ99
Contributor II

Hi,

 

I would like to make wireless with SMAC on MC13237C processor. The dev kit is 1323x-MRB-ADC with TWR-RF. I checked NXP 802.15.4 document and i could see i may refer .mcp file. The Beekit does not have an example of HCS08 SMAC. Is there any good place to have a simple example of SMAC on MC1323x?

 

thanks in advance.

YJ

0 Kudos
Reply
1 Reply

233 Views
Itzel_UV
NXP Employee
NXP Employee

Hello YJ,

 

Thanks for reaching out to us, unfortunately the product you are referring to is end of life and no longer supported, the information we have is available in Wireless Connectivity Solutions for Embedded Devices | NXP Semiconductors | NXP Semiconductors for reference however we don't have other than that.

 

This is the only information that we have available MC1323x|802.15.4 RF and 8-bit HCS08 MCU | NXP Semiconductors.

 

Regards,

Itzel

0 Kudos
Reply