Hi everyone.
I'm using a FRDM-KW38. It is introduced in the Quick Start Guide of FRDM-KW38 that when frdm-kw38 is powered on for the first time, the LED will blink, and the smart phone can be used for Bluetooth connection. Where can I download the source program of this example?
Thank you very much in advance.
Hi Liu, I hope you're doing well!
The Out-of-Box demo for the FRDM-KW38 is a BLE Beacon SDK example which allows the development kit to begin sending non-connectable advertisement packages containing the following information:
An updated version of the Beacon source code is included in the SDK package for the FRDM-KW38, now with the ability to also use Advertising Extensions, and the Coded PHY. This SDK example can be found in the following path after building, downloading and extracting the SDK from the SDK Builder site:
<…\SDK_2.6.5_FRDM-KW38\boards\frdmkw38\wireless_examples\bluetooth\beacon>
As an additional note, keep in mind that the Beacon SDK Example comes with Power Down Mode enabled by default. This can be changed by changing the value of the following macro definition to 0 in the app_preinclude.h header file:
/* Enable/Disable PowerDown functionality in PwrLib */
#define cPWR_UsePowerDownMode 0
Please let me know if you need any more information.
Take care, best regards,
Sebastian
hi, Sebastian Del Rio
Thank you very much!
it works great!
I read Bluetooth Low Energy Demo Applications User's Guide . This document is very helpful.
Thank you again for you powerfully support!
Hi,
Glad to see the example was the one you were looking for!
Please let me know if you need any more information.
Take care, best regards,
Sebastian