Hi!
I use an-1217-Router to add some endpoints. It can be built and work well if the number of endpoint less than 6.
But if i added 6 endpoints,it can be build but not work and the serial would print "!!!Trap error".
Is there some limits the number of endpoint?
SDK is "jn-sw-4170 ".
thank you!
Hi Jiazshao,
What is the process that you follow to add new endpoints?
Did you change the define ZCL_NUMBER_OF_ENDPOINTS? zcl_options.h
Regards,
Mario