Hi everybody!
I'm working in a project using the microcontroler QN9022. I have a prototype board using a 16 Mhz crystal, and the reset circuit.
To commuinicate with the board I'm using the FTDI232 board and the QN902x Studio which are working very well with the demo board qn9020_MINIDK.
I'm not achieving communicate with my prototype board, it seems that it doest enter in the boot mode whem I reset the microcontoler.
Does somebody have any idea what may be happening?
Very thanks.
Hi Oswaldo,
There are two modes in the bootloader (ISP Mode and Load Mode). It looks for a connection command from UART and SPI interface for a while to determine which mode to go.
Hi Mario!
Thank you for your answer.
The first thing i'm trying to do is to read the NVD's memory through the UART and QN902X STUDIO. I'm not achieving to do that because it can't stablish a communication.
I think that there is no problems whith the connection command because i can comunicate with the demo board qn9020_MINIDK.
I don't have an external flash, do you think that it would be a problem?
Regards,
Osvaldo
Enviado do Email do Windows
De: mario_castaneda
Enviado: segunda-feira, 15 de julho de 2019 14:14
Para: Osvaldo Nagy
NXP Community
Re: The QN9022 isn't communicating whith QN902X STUDIO
reply from Mario Ignacio Castaneda Lopez in Wireless Connectivity - View the full discussion
Hi Oswaldo,
There are two modes in the bootloader (ISP Mode and Load Mode). It looks for a connection command from UART and SPI interface for a while to determine which mode to go.
https://community.nxp.com/servlet/JiveServlet/downloadImage/2-1178107-272378/pastedImage_1.png
BL does not find Connection Command in 200ms. If no connection command found from UART and SPI interface, the bootloader enters into Load Mode.
Is it possible that you could capture the commands in this range? 200ms.
Do you have an external flash? don't you?
Regards,
Mario
Reply to this message by replying to this email, or go to the message on NXP Community
Start a new discussion in Wireless Connectivity by email or at NXP Community
Following Re: The QN9022 isn't communicating whith QN902X STUDIO in these streams: Inbox
This email was sent by NXP Community because you are a registered user.
You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences
Hi Osvaldo,
The QN9022 doesn't have an internal flash, so the commands should be different because the application will go to SRAM.
Regards,
Mario