Hello Friends
I have a project and using u-Blox module to be our connectivity,
We are trying to test Thread Rx sensitivity with Litepoint tester but no waveform available so far,
Coz the PHY layer is same with Zigbee, so I have ever tried Zigbee's waveform, it still failed,
Can somebody share your Thread Waveform ?
Thank you ...
Hi @shaun_wu
Below screenshot is the labtool command what we used,
You can see no packet has received,
I attached the waveform as well, the waveform can be captured by IQxel's SA,
We use labtool to generate Tx then record it, Litepoint helps us to transfer it to IQVSG file,
Thanks ...
Hello @Mardin
We have co-operation on 802.15.4 rf test with LitePoint. LitePoint design a zigbee test file to us, you could contact them to get the waveform file. We don't have Thread file as well. Please use Zigbee waveform to test. If still not work, you could bring you fail logs and test steps to us.
Best Regards
Shaun
Thank you Shaun
Actually we have asking LP for Thread waveform, they said no thread waveform can be provided, we have ever using buit in Zigbee waveform of LP tester, our u-Blox module still can't receive the Zigbee waveform successfully, that's why I here asking for support ...
Hello @Mardin
Thanks for your feedback. Could you share your test steps and labtool ouput to us?
Best Regards
Shaun
Hello @Mardin
Have you issued this commend:
59 1 0xface 0xabcd 0xef12
following by cmd 32?
Best Regards
Shaun
Hello @Mardin
Could you refer to following image to check your setup? Especially LitePoint side.
You could also check following things:
Issue cmd 88 to check whether interface enabled successfully.
Double check the cable is good.
Best Regards
Shaun
Hi @shaun_wu
We have tried all waveform on-hand, can't receive any packet, could you please share the waveform what you using ?
Thank you ...
Hello @Mardin
I sent you email. Please also double check mfg_tool version, if not the newest one, please use newest version to test: https://www.nxp.com/webapp/Download?colCode=NW61X2.0.0.3-18.80.2.p66.15.LABTOOLBRG&appType=license
Best Regards
Shaun