Sniffer for BLE with OM15080-K32W

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sniffer for BLE with OM15080-K32W

Jump to solution
1,094 Views
HermanLin
Contributor I

Hi @mario_castaneda

I have OM15080-K32W dongle and try to run Kinetis Protocol Analyzer with Wireshark, it only works in 802.15.4 but BLE. From KPAA, it seems the BLE filter is disabled and cannot be checked(as below screenshot).

HermanLin_0-1627017295365.png

Please advise how to use OM15080-K32W as BLE sniffer?

Need to reflash firmware? If yes, where can I get this firmware?

 

Thanks a lot!

Herman

Labels (1)
0 Kudos
Reply
1 Solution
1,067 Views
HermanLin
Contributor I

Hi Mario,

Thanks for your great support!

 

Best Regards,

Herman

View solution in original post

2 Replies
1,086 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @HermanLin,

I hope you are doing great.

We do not provide any bin file for the QN9090 to be configured as Bluetooth LE Sniffer. Sorry for any inconvenience that this may cause you.

However, the MCU that could capture these packets over the air is the USB-KW41/KW36/KW38.

Bluetooth LE Sniffer Application Update

mario_castaneda_0-1627062282656.png

Regards,

Mario

 

 

0 Kudos
Reply
1,068 Views
HermanLin
Contributor I

Hi Mario,

Thanks for your great support!

 

Best Regards,

Herman