Hi all, I have a question on programming the QN9020 development kit .
By using QPPS demo project, it will send data via "app_test_send_data" function
static uint8_t val[] = {0, '0', '1', '2','3','4','5','6','7','8','9','8','7','6','5','4','3','2','1','0'};
The result is like this:
...
00123456789876543210
10123456789876543210
20123456789876543210
30123456789876543210
...
But I want it to send one message instead of keep sending messages.
For example, QN9020 send a "Pressed" message to the client when I press a button.
By modifying which Function in order to pause the QN9020 from sending messages infinitely ?
Hello,
Have you checked the following links to see if some work for you?
Best regards,
Estephania