STA set static IP to gatewap ip(192.168.1.1) problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

STA set static IP to gatewap ip(192.168.1.1) problem

827 Views
Peter17
Contributor I

The AP gateway ip is 192.168.1.1

One client set static ip 192.168.1.1, then connect to AP

The client will be connected(get 192.168.1.1 due to static ip setting),

but it will make other clients can not access WebUI(http://192.168.1.1)

How to avoid that user using static IP assignment and set the IP to gateway ip(192.168.1.1)?

Is there any uaputl command to disconnect the specific client?

 

Thanks

0 Kudos
Reply
2 Replies

790 Views
Moran69
Contributor I

You can assign a different IP address as a static address. Usually, the first three ... The address 192.168.1.1 is often pre-assigned to the gateway router.

0 Kudos
Reply

813 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

Could you please tell me what part are you using?

Also could you please tell me if you are using a specific SDK example?

Best regards, Daniel.

0 Kudos
Reply