G2iL+ 这个系列的芯片,能实现类似硬件灭活RFID的功能吗,
我的需求是能重复使用,通过外部一个高低电平或者连接的通断控制电子标签的RF功能的启用和灭活。
Hi 烨 李 ,
This tag supports a 32-bit kill password to permanently disable the tag, but it is not recoverable, and it is not controlled externally via a GPIO pin. I am sorry but you can not use it for that purpose.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------