Replace with the same type function, an error happen

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Replace with the same type function, an error happen

668 次查看
964884134
Contributor I

As we see in the picture: when I try to change the function "....AsInitiator" and rebuilt the projet , an error happen .These two functions ,"....AsInitiator" and "....AsTarget" , should be the same type and on the same header file, why is there an error that can't find the object? Undefined Symbol ?

标记 (1)
0 项奖励
1 回复

582 次查看
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please share with me the release version of the SDK you are using? I just downloaded the latest one and the latest AN1217, just changed that line just as you have it and everything builds correctly.

target build.png


Did you modify something else?

Regards, 

Estephania 

0 项奖励