Hi,
I am developping an application on JN5169 with the ZigBee 3.0 SDK (JN-SW-4170) and one of the modules requires to have an RTOS.
A previous version of the ZigBee SDK was using JenOS, is it still possible to use it with ZigBee 3.0 SDK? Or is it possible to use any other OS?
Thank you for your help.
According to NXP support, ZigBee 3.0 stack does not support an OS.
We decided to run the other library in an external chip.
Thank you again Mario for your help.
Julien
Hi Julien,
ZigBee 3.0 applications no longer require the NXP proprietary operating system, JenOS. However, the non-OS resources that were included in JenOS (e.g. Persistent Data Manager) are included in the JN51xx Core Utilities (JCU), supplied in the JN516x ZigBee 3.0 SDK
Mario
Hi Mario,
Thank you for your answer.
I understand the ZigBee 3.0 SDK has everything to work without JenOS. However, my specific application requires an OS, because of another (non ZigBee) library I want to use which is split in several tasks.
I am also looking at removing all OS dependencies from the other library. But I think it would be easier to have one.
Do you think JenOS would be adapted in this situation?
Thank you.
Julien
Hi Julien,
The ZigBee 3.0 stack is running on bare metal. It doesn’t support an OS. However, the older version that we
provide ZHA and ZLL had OS. You can use an application note and it will be compatible with the other ZigBee products that you have.
Regards,
Mario
Hi Mario,
Why there is no support for any RTOS on JN516x microcontrollers? I`ve seen weak port of FreeRTOS to this production and nothing else. Deprecating JenOS was strange enough act.
Regards,
Igor
Hi Igor,
Sorry for any inconvenience that may cause you.
The Zigbee 3.0 stack doesn't support a OS is only bare metal, but you could look at the ZHA and ZLL, that are compatible with the Zigbee products and supports the JenOS.
Regards,
Mario