Questions about the functions of 88W8997

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Questions about the functions of 88W8997

829 Views
PeterYang_TW
Contributor I

Dear NXP support team,

Can you help us check whether 8997 supports the following functions?
1. 11ac RX A-MPDU with A-MSDU
2. 11ac RTS with BW Signaling
3. 11ac 802.11h
4. 11n 802.11h

BR,

Peter

 

0 Kudos
Reply
4 Replies

788 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello @PeterYang_TW ,

 

See below, please!

============================

1. 11ac RX A-MPDU with A-MSDU -
Yes, 11ac supports SU-AMPDU Aggregation
2. 11ac RTS with BW Signaling -
Yes, 11 ac supports RTS\CTS Bandwidth Signaling
3. 11ac 802.11h -
802.11h is supported in 8997 chipset . This feature is not specific to 802.11 ac
4. 11n 802.11h -
802.11h is supported in 8997 chipset. This feature is not specific to 802.11 n

============================

Regards,

wediong

0 Kudos
Reply

803 Views
weidong_sun
NXP TechSupport
NXP TechSupport

OK, Peter,

I will confirm these features with internal team.

 

Thanks!

Regards,

weidong

0 Kudos
Reply

656 Views
PeterYang_TW
Contributor I

Dear Support team,

 

11ac RX A-MPDU with A-MSDU

Still fails after enabling aggregation manually
In the wfa_dut.txt, looks like the sigma tool also has enabled aggregation.
Please provide solution to us.

PeterYang_TW_0-1703735914544.png

Attached VHT-5.2.56_Dec-19-2023__16-11-47 information

  • Password:123456
  • WFA_DUT: VHT-5.2.56_Dec-19-2023__16-11-47/wfa_dut.txt
  • WFA_CA: VHT-5.2.56_Dec-19-2023__16-11-47/wfa_ca.txt
  • UCC: VHT-5.2.56_Dec-19-2023__16-11-47/log_VHT-5.2.56.log
  • Sniffer: VHT-5.2.56_Dec-19-2023__16-11-47/_5256-step6
  • logcat: VHT-5.2.56_Dec-19-2023__16-11-47/logcat.txt
  • dmesg: VHT-5.2.56_Dec-19-2023__16-11-47/dmesg.txt
0 Kudos
Reply

641 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello @PeterYang_TW ,

 

Shared feedback from internal team.

check your email, please!

 

Thanks!

Regards,

weidong

0 Kudos
Reply