Phase Noise of External 32MHz for MKW01Z128

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Phase Noise of External 32MHz for MKW01Z128

896 次查看
jehangirparvere
Contributor I

We plan to use a low power external oscillator for clocking the the MKW01Zxx for metering application.

As per MKW01xxRM Reference Manual, "

An external clock can be used to replace the crystal

oscillator...." Can you please provide the phase noise requirements for such an external clock?

Thanks.

0 项奖励
回复
3 回复数

679 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Jehangir Parvereshi

Sorry for the late reply, I'm working in your case, and I was looking for information related with "noise requirements". Unfortunately we don't have requirements for this, and we don't have data for this measurements. I will continue looking information and I will keep you inform.

I could recommend you to check the designs for this chip (FRDM-KW019032, USB-KW019032) and check the 32 MHz crystal characteristics.

Sorry for the inconveniences that this may cause.

Best regards
Jorge Alcala

0 项奖励
回复

679 次查看
jehangirparvere
Contributor I

Hi Jorge:

The crystal is a passive device and crystal vendors do not provide phase noise data.

This data is available from crystal oscillator vendors. Can you please provide the part# of an
external 32 MHz crystal oscillator (TCXO) that you recommend to drive the XTAL in pin.

  Thanks.

0 项奖励
回复

679 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Jehangir Parvereshi

The one used in the FRDM-KW019032 is "EXS00A-CS02368". You can check the components in the BOM document located in downloads: "FRDM-KW019032 Design Files" package. Hope this information helps.


Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复