Hi,
following PNEV5190B evaluation board quick start guide, at some time it is needed to install the SDK. Both in MCUXpresso / Installed SDK / Available Boards and on https://mcuxpresso.nxp.com/en/select, there is not board related to 5190.
There is an SDK_2_8_0_FRDM-K82F.zip (release date 2020-07-21), which has reference for 3 boards frdmk82f, frdmk82f_clrc663, frdmk82f_pn5180.
=> Is there a dedicated pn5190 SDK somewhere?
=> If not, should I use frdmk82f_pn5180?
Regards,
解決済! 解決策の投稿を見る。
Hi @Cousin63 :
No, currently there is no dedicated package for PN5190.
For PN5190, you need to download SDK_2_8_0_FRDM-K82F.zip.
and import SDK_2_8_0_FRDM-K82F.zip into workspace, and together with nxpnfcrdlib
Regards
Daniel
Hi @Cousin63 :
No, currently there is no dedicated package for PN5190.
For PN5190, you need to download SDK_2_8_0_FRDM-K82F.zip.
and import SDK_2_8_0_FRDM-K82F.zip into workspace, and together with nxpnfcrdlib
Regards
Daniel
Hi,
which of the 3 options do I need to pick for the pnev5190 since there is no dedicated package?
frdm82_f
clrc663
pn5180
PN5190 reader library can be download from below link
PN5180 is a front end. can work with Frdm-k82f, sdk for K82f can be downloaded from below link
https://mcuxpresso.nxp.com/en/welcome
Regards
Daniel
Regards
Daniel