Hi guys,
I am working on the FRDM-KW36 board for PDE project .but have some issues to get related expert to support.
1. can i get the PDE user reference guide for the localization operation ?
2. when i setup the demo system and select the Anchor and reflect device to be ready for the measurements. but the result always showed the : SyncPacketTimeout error . what happend? is it caused by the sync access address issues? or caused by :PDE_ACCESS_ADDRESS_UNDEFINED (0x00000000U) ??
3. from the source code to see it likes the connection mode for the PDE events. but can't find where to setup the connect inteval ?
Hope to get your quick answer
Hello,
Could you please help me with the example you are using as well as which guide you are referring to ? Do you have the name or something so I can try to help you locate the file ?
Regards,
Estephania
Hello,
I believe that the release you have is custom, did you downloaded from the public MCUXpresso dashboard? Or did you get the files from somewhere else? If it was not from the public release, could you please contact the person who provided the files to you ?
Regards,
Estephania