FRIENDLY REMINDER
I just started using PNEV7462C to read and write in NTAG5 Registers. In my first example i wanted to configure the GPIO_0 and GPIO_1 as Inputs. and As i read the Register A0 i expected that both GPIOs change the status.
The commands i used in Tx data without flags are as followed :
C1A10022AF00 --> GPIO_Mode / plain Input
C1A30C000000 --> GPIO_0 and GPIO_1 as Input
C0A00 --> when i connect the GPIOs to Vcc (5v in this case i used a breadboard and some jumpers for this set up) the card response i get is : 03C80000 but I'm expecting 03D80000 ( GPIO1_IN_STATUS bit didn't change ) i tried many configurations like disabling the recievers , and use just the GPIO_1 as Input but the GPIO1_IN_STATUS bit in register A0 still don't change at all though I'm connecting it to Vcc.
Can someone help me with this problem.
Thank you in Advance.
Please, kindly check my response in: https://community.nxp.com/t5/Wireless-Connectivity/NTAG5-with-PNEV7462C-Board-using-NFC-Cockpit/m-p/...