NFC communication error due to PH_ERR_COLLISION_ERROR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC communication error due to PH_ERR_COLLISION_ERROR

Jump to solution
616 Views
VasuVirpariya
Contributor II

We are using PN7462 to read the type2 tag. We successfully establish the connection between them. We are reading tags at every 500ms. However, after approximately 2-3 minutes, we noticed that the connection was lost. After we debugged we discovered that the hal library for PN7462 returned a collision error(PH_ERR_COLLISION_ERROR).

What could be the cause of this error?

Tags (2)
0 Kudos
Reply
1 Solution
395 Views
VasuVirpariya
Contributor II

It was a hardware issue.

View solution in original post

0 Kudos
Reply
2 Replies
396 Views
VasuVirpariya
Contributor II

It was a hardware issue.

0 Kudos
Reply
572 Views
Fabian_R
NXP TechSupport
NXP TechSupport

Hello, my name is Fabian, I've been assigned to support your case.
I appreciate your interest in our products.
Could you please clarify which example are you using and, if the application isn't causing a failure in the memory of the PN7462 or, creating some sort of bottleneck in the respective controller?
I have to highly recommend that you take a look at the memory management since, these are examples for testing purposes and to show how the API is used but, I'm sure there is a lot of improvement room.

Best Regards,
Fabian
0 Kudos
Reply