Hello,
Had a couple of questions about using NFC and the LPC54114. On my stand-alone board I want to use NFC to enter/tweak some parameters, then start my application code running:
1 - As far as I can tell the LPC54114 does not contain any native NFC support. Can NXP suggest a suitable NFC device to build into my LPC54114 system ?
2 - Is there an NXP tool I can use to generate the NFC application on my smart phone ?
3 - I've read some of the documentation but just in case I've missed something, is there some documentation/app note/examples that describes this scenario ?
Regards,
Jim
Hello,
NTAG I²C provides an interface between NFC and I²C, for more information, please refer to the following link: NTAG I2C | NXP
For mobile development, please refer to TapLinx: TapLinx | MIFARE
Hope it helps.
BR,
Ivan.