NFC and LPC54114

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC and LPC54114

462件の閲覧回数
jameswhitney
Contributor II

Hello,

Had a couple of questions about using NFC and the LPC54114. On my stand-alone board I want to use NFC to enter/tweak some parameters, then start my application code running:

1 - As far as I can tell the LPC54114 does not contain any native NFC support. Can NXP suggest a suitable NFC device to build into my LPC54114 system ?

2 - Is there an NXP tool I can use to generate the NFC application on my smart phone ?

3 - I've read some of the documentation but just in case I've missed something, is there some documentation/app note/examples that describes this scenario ?

Regards,

Jim

0 件の賞賛
1 返信

420件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

NTAG I²C provides an interface between NFC and I²C, for more information, please refer to the following link: NTAG I2C | NXP 

For mobile development, please refer to TapLinx: TapLinx | MIFARE 

 

Hope it helps.

BR,

Ivan.

0 件の賞賛