NFC Cockpit connect error with CLEV6630B

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC Cockpit connect error with CLEV6630B

ソリューションへジャンプ
1,262件の閲覧回数
jenny_nfc
Contributor I

hi,

  It's the 1st time I use CLEV6630B(RC663).

  The Cockpit v6.50 and VCOM.bat have been installed.

   But when Cockpit opened,Log Monitor says:

ERROR:ServiceFactory:Bal, Hal, OSal Initialization (VCOM_RC663 @COM3) Failed with GENERIC,USE_CONDITION

  How can I solve the problem?Thanks.

CockpitError.PNG

タグ(1)
0 件の賞賛
返信
1 解決策
1,222件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello @jenny_nfc .

Thanks for your information.
In order to better service for you, would you please kindly provide the below information?
Firstly. Did you follow the step of 3. Software as the AN11022 as the link?
URL:https://www.nxp.com.cn/docs/en/application-note/AN11022.pdf.
Secondly. Did you test Cockpit V6.3 and  has the same question?

 

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
153件の閲覧回数
imx8-mdt
Contributor I

Hi  

have you addressed this connection issue?

I have the same issue to connect CLEV6630B with Cockpit v8.0.

I think the vcom driver has been installed ,as I can see the COM30 show up in my windows10 device manager.

I just tear down the package of CLEV6630B today. so I think the default firmware in it should work for Cockpit reading/writing.

 

Could anyone help on this? Thanks

imx8mdt_0-1716545482794.png

 

タグ(1)
0 件の賞賛
返信
1,223件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello @jenny_nfc .

Thanks for your information.
In order to better service for you, would you please kindly provide the below information?
Firstly. Did you follow the step of 3. Software as the AN11022 as the link?
URL:https://www.nxp.com.cn/docs/en/application-note/AN11022.pdf.
Secondly. Did you test Cockpit V6.3 and  has the same question?

 

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛
返信