hi,
It's the 1st time I use CLEV6630B(RC663).
The Cockpit v6.50 and VCOM.bat have been installed.
But when Cockpit opened,Log Monitor says:
ERROR:ServiceFactory:Bal, Hal, OSal Initialization (VCOM_RC663 @COM3) Failed with GENERIC,USE_CONDITION
How can I solve the problem?Thanks.
解決済! 解決策の投稿を見る。
Hello @jenny_nfc .
Thanks for your information.
In order to better service for you, would you please kindly provide the below information?
Firstly. Did you follow the step of 3. Software as the AN11022 as the link?
URL:https://www.nxp.com.cn/docs/en/application-note/AN11022.pdf.
Secondly. Did you test Cockpit V6.3 and has the same question?
Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------
Hi
have you addressed this connection issue?
I have the same issue to connect CLEV6630B with Cockpit v8.0.
I think the vcom driver has been installed ,as I can see the COM30 show up in my windows10 device manager.
I just tear down the package of CLEV6630B today. so I think the default firmware in it should work for Cockpit reading/writing.
Could anyone help on this? Thanks
Hello @jenny_nfc .
Thanks for your information.
In order to better service for you, would you please kindly provide the below information?
Firstly. Did you follow the step of 3. Software as the AN11022 as the link?
URL:https://www.nxp.com.cn/docs/en/application-note/AN11022.pdf.
Secondly. Did you test Cockpit V6.3 and has the same question?
Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------