Hi to all,
Hope you all are doing good in this tuff time.
I am working with the controller kw41z512 controller with connectivity SDK(MKW41Z_ConnSw_1.0.2) and KDS.
I am trying to connect multiple central with a single peripheral using the application note (AN12405).
But the following lines draw my attention.
#if (gAppMaxConnections_c > 1)
#error "The application does not support more than 1 connection"
#endif
I want to know if the current SDK supports the multiple connection feature or not?
Solved! Go to Solution.
Hi,
Please download the latest sdk in https://mcuxpresso.nxp.com/en/select. Notice that KW41 can only connect 2 device at the same time.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi,
Please download the latest sdk in https://mcuxpresso.nxp.com/en/select. Notice that KW41 can only connect 2 device at the same time.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------