[MKW36A512VFP4] Antenna Diversity

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[MKW36A512VFP4] Antenna Diversity

Jump to solution
312 Views
deega_jung
Contributor III

Dear NXP support team,

Please let me know if KMW36 supports antenna diversity.
If it support antenna diversity, please share the related reference circuit and guide for me how to use about software and hardware.

Thanks,

Deega Jung

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
296 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello,

 

Thank you for contacting NXP support.

The antenna diversity is implemented with two antenna’s which are separated and have offset orientation which allows the transceiver to statistically improve the chance to receive the RF signal outside the dynamic range of the system.

 

The KW36 has support only for one antenna so the antenna diversity is not supported on this chip, on the KW36-FRDM has a PCB F-antenna which can be bypassed to test via SMA connection.

We provide an schematic and design file that can be located on the FRDMKW36. This provide the information on how this is configured in the board.

Please let me know if there is anything else where I can help you.

View solution in original post

0 Kudos
Reply
1 Reply
297 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello,

 

Thank you for contacting NXP support.

The antenna diversity is implemented with two antenna’s which are separated and have offset orientation which allows the transceiver to statistically improve the chance to receive the RF signal outside the dynamic range of the system.

 

The KW36 has support only for one antenna so the antenna diversity is not supported on this chip, on the KW36-FRDM has a PCB F-antenna which can be bypassed to test via SMA connection.

We provide an schematic and design file that can be located on the FRDMKW36. This provide the information on how this is configured in the board.

Please let me know if there is anything else where I can help you.

0 Kudos
Reply