Labtool - 88W8997 - iMX8M Linux Host

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Labtool - 88W8997 - iMX8M Linux Host

1,877 Views
amaggs
Contributor I

Hi There,

I have obtained Labtool but it is unclear on what needs to be running on the iMX8M Linux host system for Labtool to connect to.

 

I am assuming there is some application that needs to be cross compiled for the particular hardware/software configuration of the EVB noted above for Labtool to connect to?...

 

Any help is greatly appreciated!

 

Thanks,

Anthony

0 Kudos
Reply
6 Replies

1,256 Views
RichardFelician
Contributor I

Has anyone followed up on this issue we got the same result

 

0 Kudos
Reply

1,866 Views
shaun_wu
NXP TechSupport
NXP TechSupport

Hello @amaggs 

You could refer to following document for 8997 labtool setup:

 

Best Regards

Shaun

0 Kudos
Reply

1,850 Views
amaggs
Contributor I

Hi Shaun,

Thank you very much for your response. Yes, I have reviewed this document. This document does a very good job of documenting what needs to be done when a bridge PC is being used but in our case the DUT is a "88W997 System"

Our host processor which is part of the 88W997 System is an iMX8M running Linux.

What needs to be running on our host and is there documentation for setting up our host? Should we consider our iMX8M as the bridge and follow bridge PC instructions?... I am not sure if this is possible, I will speak with embedded programmers internally.

 

Any help and assistance is greatly appreciated.

 

Thanks,

Anthony

 

0 Kudos
Reply

1,832 Views
shaun_wu
NXP TechSupport
NXP TechSupport

Hello @amaggs 

You are right. Please run mfg_bridge on i.mx platform, run Labtool on host PC. Host PC and i.mx platform should under same subnet.

0 Kudos
Reply

1,779 Views
amaggs
Contributor I

Hi Shaun,

We were able to port mfgbridge to run on iMX8M. We are also able to run Labtool and it seems to be communicating with mfgbridge app. However, I cannot get any TX output when I run "802.11n Test Sequences - 5.2.4.1 Tx on Selected Path, 2.4 GHz, 20 MHz Bandwidth, MCS7 Data Rate" from Labtool user guide.

 

Please see Labtool commands and responses below.

 

Thanks,

Anthony

 

Name:      Dut labtool

Version:    1.0.0.173

Date:      Jul 7 2020 (00:57:53)

 

Note:

 

1. =========WiFi tool=============

2. =========BT  tool=============

 

Enter CMD 99 to Exit

 

Enter option: 1

Name:      DutApiClass

Interface:   EtherNet

Version:    1.0.0.173

Date:      Jul 7 2020 (00:56:49)

 

Note:

 

Dut's IP 192.168.0.10:9930

Host's IP 192.168.0.100:9931

DutIf_UdpIp::delay 0

DutIf_UdpIp::vg_IfSpy 0

_WSAStartup _socketCount=1

TCP connecting...

 DutIf_InitConnection: 0x00000000

--------------------------------------------------------

        W89xx (802.11a/g/b/n/ac) TEST MENU

--------------------------------------------------------

Enter option: 88

DLL Version : 1.0.0.173

LabTool Version: 1.0.0.173

 DutIf_GetFWVersion: 0xFFFFFFF9

SOC OR Version: 0.0   Customer ID:  0

RF OR Version: 0.0   Customer ID:  0

Enter option: 35

 DutIf_AdjustPcktSifs: 0xFFFFFFF9

Enter option: 10 3 3

 DutIf_SetTxRxPath: Tx path to 3 : Rx path to 3 : status 0xFFFFFFF9

Enter option: 30 0

 DutIf_SetModeAG: 0xFFFFFFF9

Enter option: 112 0

DutIf_SetChannelBw: 0xFFFFFFF9

Enter option: 12 6

 DutIf_SetRfChannel: 0xFFFFFFF9

Enter option: 22 3 6 10 2

 DutIf_SetRfChannel: 0xFFFFFFF9

Enter option: 35 1 22 1 100 F00

 DutIf_AdjustPcktSifs: 0xFFFFFFF9

    TRPC ID: 0xffffffff

Enter option: 35

 DutIf_AdjustPcktSifs: 0xFFFFFFF9

Enter option:

0 Kudos
Reply

1,770 Views
shaun_wu
NXP TechSupport
NXP TechSupport

Hello @amaggs 

Could you share driver version to us?

0 Kudos
Reply