LTE3401H allowed power at the output

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LTE3401H allowed power at the output

Jump to solution
643 Views
NirAlon
Contributor I

Hello all,

In my design, I use the LTE3401H at 3V.

There is a RX path and TX path with maximum +13dBm TX power

The LNA is always on, also during TX.

The RF isolation of the RF switch of about -20dB from TX to RX path, so actually there is a -7dBm of power reaching to the LNA output during TX.

Is that ok?

Should I refer to maximum output power values in order to answer this question?

NirAlon_0-1708672118559.png

Thanks!

Nir

0 Kudos
Reply
1 Solution
568 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

Yes, I refer to S12, which is the reverse voltage gain.

View solution in original post

0 Kudos
Reply
3 Replies
605 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

I suppose the S12 is asked in Gain mode!
Derived from the Sparameters we see:

ErikaC_0-1708985171744.png

In DS we see typ. -30dB, I do not have data on the spread on this. Expect it to be limited.

 

0 Kudos
Reply
579 Views
NirAlon
Contributor I

Hi Erika,

Just to be clear, I'm asking what is the allowed power at the LNA output, resulting from TX power -20dB of RF switch isolation.

NirAlon_0-1709096734671.png

your answer was referring to this situation?

Thanks

Nir

0 Kudos
Reply
569 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

Yes, I refer to S12, which is the reverse voltage gain.

0 Kudos
Reply