Hi
1.Hardware shall support secure boot mechanism to ensure integrity and authenticity of the firmware or operating system images. For example, it checks the digital signature of the images during startup phrase.
2.Secure boot should be based on a hardware trusted root such as HSM/SE/TPM.
3.If the firmware is tampered with or invalid firmware is brushed in, or the firmware cannot pass the integrity and signature verification for any reason, the ECU shall automatically roll back to the previous firmware version or refuse to start.
Can you provide some information and reference methods on how we should operate secure boot? Does this need to start operation edgelock enclave? I looked up some of your SPSDK secure boot reference routines. But it is not clear what their specific principles and motives are.
Best regards.
# uploads
I
#! blhost $UART COCTION write memorv OxO SHBI OUIPUT FILE
! blhost -p COM18 flash-erase-all
Response status = 0 (Ox0) Success.
In
[45]: ! blhost -p COM18 write-memory Ox0 workspace/lBI/my_mbi.bin
Writing memory
Response status = 0 (Ox0) Success.
Response word 1 = 1040836 (Oxfelc4)
In
[46]: ! blhost $UART_CONNECTION reset
Response status = 0 (Ox0) Success.
4.SEC tool about KW45, where is it? Can you provide it?
5.As follow shown , in ISP mode, how are these instructions sent out through the serial port? What software is used, what kind of environment and tools are needed, and it is best to have specific operation methods?
"This section explains the general protocol for the packet transfers between the host and the ROM Bootloader. The description
includes the transfer of packets for different transactions, such as commands with no data phase and commands with incoming
or outgoing data phase. The next section describes various packet types used in a transaction" 10.4 In-System Programming protocol
Hello,
Please find the answer to your questions below:
In the AN13838 in the chapter 6.4 you will find the image verification, where the process of how the image is validated and use is explain in a deeper way.
Yes, also on the AN13838 Chapter 6 you will find the differences between signed image (6.2), sb3 file (6.3), and unsigned or plain image (6.1).
Sure we have the following application note AN14109, where is explained the usage of the SEC Tool.
Also please find the link to the Secure Provisioning Tool.
Please let me know if there is anything else where I can help you.
Hello,
Thank you for contacting NXP support.
Regarding your questions, you can find more detailed information on Security Reference Manual on the Chapter 9.3 you will find the features of BOOT Rom in a more detailed way, also is in the Chapter 9.3.7 you will find a more detailed information on how the secure boot is used.
Please let me know if there is anything else where I can help you.
Hello,
Please help me by login into your NXP account in order to have access to download this document.
Also we have a couple of application notes related to secure boot, located on the KW45 documentation under the secure files perspective. If you can please help me by verifying you have access to this documentation (you need to be log in into your NXP account).
Please let me know if you have access.
Hello!
I need your answers and support on the following two matters.
1. KW45 starts safely. What should I pay attention to if I use RoTKTH generated by NBU before? Why I used the previous key to generate the signature image, the security boot failed. I changed the state of FUSE to Security world closed. How can I determine what went wrong inside the security boot? I need your email or phone support.
2.Can NBU files (including general.sB3 files) be upgraded by Bootloader? If yes, can you provide relevant documents and software information? Is the method mentioned in AN14003 related to the NBU file upgrade by Bootloader? In addition, could you please provide the projects and tools mentioned in this document for our reference? Is the download mode supported by the CAN bus?
Hello,
Answering your questions:
Please let me know if you have any other question.
Hi,
I meet the same problems that KW45 can't jump to application and always run the ROM BOOT when I change KW45 lifecycle to "OEM SECURE WORLD CLOSED". I checked that the RoTKTH and SB3KDK is wrote in KW45 fuse right and KW45 can execute the "wireless uart" application before changing the life cycle.The way I burn the application firmware is that I generate the application sb3 image using the same keys(RoTKTH and SB3KDK) in KW45 fuse and send the application sb3 image to KW45 through ISP. How can kw45 execute the application code in "OEM SECURE WORLD CLOSED" lifecycle?