KW41Z with external amplifier

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW41Z with external amplifier

Jump to solution
1,100 Views
lukaszgesieniec
Contributor II

Where can I find software example how to use KW41Z with external amplifier? My application uses BLE and Thread.

I have to know how configure Wireless Connectivity stack to control RX_SWITCH and TX_SWITCH pads connected to my external amplifier.

I have connected external amp this way (fig from kw41z reference manual):

pastedImage_1.png

Labels (1)
0 Kudos
Reply
1 Solution
882 Views
gerardo_rodriguez
NXP Employee
NXP Employee

Hello Lukasz,

To enable the TX/RX switch pins, you need to configure the mux of the pins, the timing registers for the TX/RX switch signals and enable the RX/TX_SWITCH on the FAD_CTRL register.

You can use the following code as reference. Include fsl_port.h and Phy.h.

    PORT_SetPinMux(PORTC,2u,kPORT_MuxAlt2); // PTC2 as TX_SWITCH
    PORT_SetPinMux(PORTC,3u,kPORT_MuxAlt2); // PTC3 as RX_SWITCH

    // TX_SWITCH output is derived from TSM output gpio2_trig_en
    // Timings for assertion/de-assertion for GPIO2_TRIG_EN
    XCVR_TSM->TIMING49 = 0xFFFFFF01;

    // RX_SWITCH output is derived from TSM output gpio2_trig_en
    // Timings for assertion/de-assertion for GPIO3_TRIG_EN
    XCVR_TSM->TIMING50 = 0xFF01FFFF;

    // Enable RX/TX_SWITCH
    PhyPlmeSetANTPadStateRequest(FALSE, TRUE);

Regards,

Gerardo

View solution in original post

2 Replies
883 Views
gerardo_rodriguez
NXP Employee
NXP Employee

Hello Lukasz,

To enable the TX/RX switch pins, you need to configure the mux of the pins, the timing registers for the TX/RX switch signals and enable the RX/TX_SWITCH on the FAD_CTRL register.

You can use the following code as reference. Include fsl_port.h and Phy.h.

    PORT_SetPinMux(PORTC,2u,kPORT_MuxAlt2); // PTC2 as TX_SWITCH
    PORT_SetPinMux(PORTC,3u,kPORT_MuxAlt2); // PTC3 as RX_SWITCH

    // TX_SWITCH output is derived from TSM output gpio2_trig_en
    // Timings for assertion/de-assertion for GPIO2_TRIG_EN
    XCVR_TSM->TIMING49 = 0xFFFFFF01;

    // RX_SWITCH output is derived from TSM output gpio2_trig_en
    // Timings for assertion/de-assertion for GPIO3_TRIG_EN
    XCVR_TSM->TIMING50 = 0xFF01FFFF;

    // Enable RX/TX_SWITCH
    PhyPlmeSetANTPadStateRequest(FALSE, TRUE);

Regards,

Gerardo

882 Views
lukaszgesieniec
Contributor II

Thank you!

0 Kudos
Reply