The sum of AppAdvertisingData and AppScanRspData cannot be greater than 31 bytes.
In my understanding,The maximum value of AppAdvertisingData is 31 bytes, The maximum value of AppScanRspData is also 31 bytes, The sum of the two is 62 bytes, why can kw38 only reach 31 bytes.
Please help to answer, thank you
Hi,
I will be helping you with your question.
Could you tell me what example is used with the version of the SDK and give me more details on the manipulation of the AppAdvertisingData and AppScanRspData?
Regards,
Itzel
Hello,
Could you tell me the version of SDK that you're using?
On the other hand, could you please share with me the code where it has being modified and declare the variable
scanRspStruct? If you prefer it can be done in a private message.
Regards,
Itzel.