KW38:the sum of AdvertisingData and ScanRspData

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KW38:the sum of AdvertisingData and ScanRspData

75件の閲覧回数
LISI1
Contributor I

The sum of AppAdvertisingData and AppScanRspData cannot be greater than 31 bytes.

In my understanding,The maximum value of  AppAdvertisingData is 31 bytes, The maximum value of AppScanRspData is also 31 bytes, The sum of the two is 62 bytes, why can kw38 only reach 31 bytes.

 

Please help to answer, thank you

0 件の賞賛
1 返信

10件の閲覧回数
Itzel_UV
NXP Employee
NXP Employee

Hi,

I will be helping you with your question.

 

Could you tell me what example is used with the version of the SDK and give me more details on the manipulation of the AppAdvertisingData and AppScanRspData?

 

Regards,

Itzel

0 件の賞賛