KW35/36 to KW37/38/39 migration: flashloader UART0 pinning

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW35/36 to KW37/38/39 migration: flashloader UART0 pinning

1,166 Views
matthieu_baudry
NXP Employee
NXP Employee

User will be concerned by this note in the following cases: 

- migration from KW35/36_HVQFN48 Wettable Flank package version to KW37/38/39 

- Flashloader is used via UART0 interface 

So, KW35/36_HVQFN48 Wettable Flank package version and KW37/38/39 are pin to pin compatible. 

In order to keep more flexibility on KW37/38/39 pins used for the flashloader have been updated for UART0.

KW35/36 UART0 pin: PTC2_UART0_RX, PTC18_UART0_RX

KW37/38/39 UART0 pin: PTC6_UART0_RX, PTC7_UART0_RX    (PTC18 is kept for SPI only)

pastedImage_1.png

The flashloader is programmed in the NXP factory to allow the user to dowload its own code. 

To know more on Flashloader: https://community.nxp.com/docs/DOC-341224

To know more on KW37/38/39: KW39/38/37 32-bit Bluetooth 5.0 Long-Range (please refer to Reference MAnual for Flasloader interface listing)

User migrating from KW35/36_HVQFN48 Wettable Flank package version to KW37/38/39 and using flashloader via follwing interfaces are not concerned: I2C, SPI or CAN

Labels (2)
0 Replies