1.How can I use WWAH cluster on JN5169 and JN5189 projects?.
2.I noticed that the JN5189 project had this WWAH cluster, but I added it to zcl_options.h to show when compiled.How do I compile successfully?
3.In addition, how to transplant to the JN5169 project?
Hi @LChll,
You could implement the WWAH Cluster in the JN5169, there is available the cluster in the JN5189.
Please look at the next community post.
https://community.nxp.com/t5/Wireless-Connectivity-Knowledge/ZigBee-3-0-Adding-Clusters/ta-p/1104282
I strong recommend to look at the JN5189 MCU, it is the current device for the Zigbee Stack.
Regards,
Mario