JN5189: NFC communication with Android.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

JN5189: NFC communication with Android.

718 次查看
usaygo
Contributor III

Hello,

Is it possible for JN5189's NFC communicating with Android smart phones? If feasible, what is the better way for `getting started'? (e.g. any good example? Trying PN7150 firstly then go back to JN5189? ...)

Thanks and regards!

0 项奖励
2 回复数

714 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

1 Yes. 

2 What the role you want the mcu play? Reader(Read the info from phone) or Tag(Provide the data for phone to read)? Do you have the develop board?

3 PN7150 is a reader. So you want to connect the JN5189 with PN7150? And read the data form phone? If so, you should concern about the porting the nfc lib to your mcu. Link for you to refer.

 

 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励

686 次查看
usaygo
Contributor III

Hello TIC,

Thanks for the comment.

2 What the role you want the mcu play? Reader(Read the info from phone) or Tag(Provide the data for phone to read)? Do you have the develop board?

Might be both, but the Reader is prioritized. For example, Phone as configurator: store some setting information on Phones and provide them to the Reader device.

I have DK6 of JN5164 and it seems to have both Reader/Writer functions.

3 PN7150 is a reader. So you want to connect the JN5189 with PN7150? And read the data form phone? If so, you should concern about the porting the nfc lib to your mcu. Link for you to refer.

Sorry, I just guessed that starting with well-proven PN7150 is much easier to understand technical  issues. After then going back to JN5189-DK6. Thanks for the Link, it seems good information

0 项奖励