JN5169 Zigbee

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JN5169 Zigbee

1,816 Views
berniecheah
Contributor I

Hi,

I understand from the Iot Modular framework - Volansys Gateway (as attached), the Zigbee module can connect up to a minimum of 255 nodes per gateway.

Can I also check, with the Zigbee chip itself, how many nodes can it connect? If I were to set up/program my own module and not use the give source code by NXP or Volansys.

Can't seem to find this specification from the JN5169 datasheet.

0 Kudos
Reply
1 Reply

1,070 Views
ovidiu_usturoi
NXP Employee
NXP Employee

Hi berniecheah‌,

Definitely  you can use the chip itself to validate/build a new ZigBee network.

My recommendation is to start from an application note provided by NXP:  ZigBee 3.0|NXP .

(To flash the chip you can use a FTDI cable. The following user guide explained the steps to flash the board: https://www.nxp.com/docs/en/user-guide/JN-UG-3099.pdf or you can use directly the Beyond Studio for NXP -> Devices->Program Device).

If you need more details, let us know.

Regards,

Ovidiu

0 Kudos
Reply