Hi,
I'm not able to get any of JN-AN-1217, JN-AN1220 or JN-AN-1229 projects imported.
I've selected the 5169 module for its low power consumption and range.
I eventually found this page: https://www.nxp.com/products/wireless/proprietary-ieee-802.15.4-based/zigbee/zigbee-3.0:ZIGBEE-3-0 and downloaded JN-SW-4141 v1308 and as per JN-UG-3098 v1.2 I installed it. Looked good. No issues using the default c:\NXP directory on windows 10.
I then installed JN-SW-4170 and following UG-3098 I added the Zigbee Plugins. (This is confusing as the documentation for ZigBee 3 says JenOS is not used any more yet there is a config plugin for it in 4170???) UG-3098 Chapter 1.2.3 step 4 refers to SW-4168 rather than SW-4170. The same zigbee URL page above says to use version 1.3 of 3098 but the link on that page provides V1.2?? I assumed I could substitute 4170 for 4168 as the SDK.
Following Chapter 2.2 of 3098 when I try to import any of the JN-ANs listed above there are no projects to open.
My ultimate goal is it have approximately 30 sleeping end devices reporting temperature readings and cell battery voltage to a coordinator.
I'd really appreciate some guidance to get me started. What I hoped would be a simple project has turned into a never ending set of problems.
Thanks ...Laurie:{)
Hi Mario,
Thanks for your reply but I've seen that already.
Please confirm
1) that version 1.2 is the latest for UG-3098
2) 4170 is the replacement for 4168 as the SDK
Trying to import the ANs I unzipped them and then used the zip that is within the directory within the AN as the target for the import.
I tried just importing the 5169 project (as 517x is not supported in beyond) but when I tried that all the directories in the project can't be opened and (from the file system) there are no files in the directories.
Thanks ...Laurie:{)
Hi Laurie,
1) that version 1.2 is the latest for UG-3098
Yes, is the latest version.
2) 4170 is the replacement for 4168 as the SDK.
The 4170 is for Zigbee 3 and the 4168 is for Zigbee HA or LL.
Please unzip the AN and be sure that not have another folder. For example:
C:\NXP\bstudio_nxp\workspace\JN-AN-1217-Zigbee-3-0-Base-Device.
Please let me know If you still have issues on this.
Regards,
Mario
Hi Laurie,
Please look at the next community post
https://community.nxp.com/docs/DOC-340028
Regards,
Mario