Dear Sirs,
My Timer3 callback was not run. Is there any problem below?
vAHI_Timer3RegisterCallback(vHwTimer3IntCallback);
vAHI_TimerEnable(E_AHI_TIMER_3, 4, TRUE, TRUE, FALSE);
vAHI_TimerConfigureOutputs(E_AHI_TIMER_3, FALSE, TRUE);
vAHI_TimerClockSelect(E_AHI_TIMER_3, FALSE, TRUE);
vAHI_TimerStartSingleShot(E_AHI_TIMER_3, 6250, 62500);
PUBLIC void vHwTimer3IntCallback(uint32 u32DeviceId, uint32 u32ItemBitmap)
{
u8AHI_TimerFired(E_AHI_TIMER_3);
DBG_vPrintf(TRUE, "Timer3Cb(id=0x%08x, bit=0x%08x)\n", u32DeviceId, u32ItemBitmap);
}
Solved! Go to Solution.
edit the ISR file irq_JN516x.S